You are here: Getting Started > Advanced Project Creation > Define Scheduling > About Parent-Child Relationships and Execution Order

About Parent-Child relationships and execution order

The SFC"Sequential function chart" It can be used to program processes that can be split into steps. The main components of SFC are: - Steps with associated actions - Transitions with associated logic conditions - Directed links between steps and transitions Section allows for editing the period and phase values of parent and child programs. Parent and child programs follow certain rules:

To understand the last rule, consider the following Cycle example. There are three parent programs, each with a number of child programs. All parents are executed, followed by the children, in order. The actual flow is illustrated below the image.

Parent1
 Parent2
    Parent3
       Parent1_Child1
          Parent1_Child1_Child1
             Parent1_Child2
                Parent1_Child2_Child1
                   Parent2_Child1
                      Parent2_Child1_Child1
                         Parent3_Child1
                            Parent3_Child1_Child1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™